Max_Current

Index.Sub 2005.2H
Data Type Unsigned16
Access Read/Write
PDO Mappable RX_PDO (1)
Unit

milliamperes (mA)

Range

0 to Max drive current

Default Value 0
Store Supported Yes
Description

It sets the motor’s current when running at constant speed. During acceleration and deceleration, the Boost_Current is automatically set.

This object is used for Open Loop feature.

Notes

(1) Available with firmware V02r20 or superior.

The current set is the Irms current.